When I checked the AM335X SK board (By connecting to PC and using Linux commands), I Could find that number of Endpoints associated with USB are 2 and supporting maximum size of 512 Bytes. Also the VID and PID of the USB module are different than those mentioned in the AM335X TRM Rev. M. May i know the reason for this discrepancy with regards to AM335X technical reference manual ?