Hi everyone,
I'm trying to modify the encoding demo code supplied with the dm6467t evaulation board to capture video in SD format (PAL, 576i or 576p @50Hz), without success.
Is it possible? What kind of issues may I find in the way?
Some ideas:
- Is the clock of the evaluation board fed to the TVP5147 suited to capture that format?
- Can the clock be reprogrammed to fit any Video standard?
- Is it possible to load TVP7002 and TVP5147 kernel drivers simultaneously in the latest kernel versions? What I learnt today is that there may be an I2C address conflict between those chips. Is that fixed?
Any advice will be appreciated!
Gerard.