This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Processor selection

Hi ALL,

                      This is my requirement ..............i.e.

 2 * ethernet interfaces (10/100Mbit)

2 * RS232/422/485 serial lines(modem lines are not necessary in RS232 mode)

8 * gpio lines

2 * audio interface(independent 600 ohm balanced inputs and outputs to be interfaced with common radio equipment)

1 * USB Console interface

1 * USB host interface

1 * reset(switch) interface

1 * power indicator LED interface

min 2 * status led interface

wide input dc power supply

form factor: TBD but no larger than PC-104 form factor

BSP : Linux

Environment specifications : industrial spec

we would need the audio interfaces to be accessible as ALSA devices for our applications to work properly. We would also need the vocoder to work natively with pjsip application(and preferably with asterisk framework).

                       

Please help me choosing a good ti processor for the above requirement.

regards,

ravishankar.