This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x WinCE gigabit ethernet throughput issue

I searched the below link with the AM335x under the wince7 gigabit ehternet  throughput is upto 139.92Mb/s(FTP put) and I am wondering why the AM335x has the gigabit ethernet port but the real test performance is not well.What is its cause? Is the WINCE7 OS issue (Under Linux is around upto 300Mb/s) ? or the BSP or AM335x HW issue or the others ?

Is there any method to improve the AM335x gigabit ethernet speed ? Thanks for your help.

 http://processors.wiki.ti.com/index.php/WinCE_Comparative_Benchmarks#Ethernet_Tests