This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Download error

Other Parts Discussed in Thread: TMS320C6748

Hardware platform  : tms320c6748

Emulator: xds200

I can't download program After updating the CCS. The error shows as blow :

ICEPICK_C: Error initializing emulator: (Error -1056 @ 0x0) A firmware update is recommended for the XDS2xx debug probe. For XDS200 probes, update the firmware using the xds2xx_conf utility found in the .../ccs_base/common/uscif/xds2xx directory of the CCS installation. View the ReadMe.txt file there for instructions. For other XDS2xx variants, follow the manufacturer's instructions for updating the firmware. (Emulation package 6.0.228.0) 

How can I do to solve this problem?

  • Hi,

    Please download and install the emulation package , 6.0.228.0


    You would be able to connect the target to CCS.

  • Thanks for your answer,

    I have download and install the emulation package, 6.0.228.0.

    The error still exists.

    But It's succeed when I test the connection the target to CCS.

    [Start: Texas Instruments XDS2xx USB Debug Probe_0]
    
    Execute the command:
    
    %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
    
    [Result]
    
    
    -----[Print the board config pathname(s)]------------------------------------
    
    C:\Users\FANXUC~1\AppData\Local\TEXASI~1\
        CCS\install\0\0\BrdDat\testBoard.dat
    
    -----[Print the reset-command software log-file]-----------------------------
    
    This utility has selected a 560/2xx-class product.
    This utility will load the program 'xds2xxu.out'.
    The library build date was 'Apr 28 2016'.
    The library build time was '02:18:13'.
    The library package version is '6.0.228.0'.
    The library component version is '35.35.0.0'.
    The controller does not use a programmable FPGA.
    The controller has a version number of '13' (0x0000000d).
    The controller has an insertion length of '0' (0x00000000).
    This utility will attempt to reset the controller.
    This utility has successfully reset the controller.
    
    -----[Print the reset-command hardware log-file]-----------------------------
    
    This emulator does not create a reset log-file.
    
    -----[Perform the Integrity scan-test on the JTAG IR]------------------------
    
    This test will use blocks of 64 32-bit words.
    This test will be applied just once.
    
    Do a test using 0xFFFFFFFF.
    Scan tests: 1, skipped: 0, failed: 0
    Do a test using 0x00000000.
    Scan tests: 2, skipped: 0, failed: 0
    Do a test using 0xFE03E0E2.
    Scan tests: 3, skipped: 0, failed: 0
    Do a test using 0x01FC1F1D.
    Scan tests: 4, skipped: 0, failed: 0
    Do a test using 0x5533CCAA.
    Scan tests: 5, skipped: 0, failed: 0
    Do a test using 0xAACC3355.
    Scan tests: 6, skipped: 0, failed: 0
    All of the values were scanned correctly.
    
    The JTAG IR Integrity scan-test has succeeded.
    
    -----[Perform the Integrity scan-test on the JTAG DR]------------------------
    
    This test will use blocks of 64 32-bit words.
    This test will be applied just once.
    
    Do a test using 0xFFFFFFFF.
    Scan tests: 1, skipped: 0, failed: 0
    Do a test using 0x00000000.
    Scan tests: 2, skipped: 0, failed: 0
    Do a test using 0xFE03E0E2.
    Scan tests: 3, skipped: 0, failed: 0
    Do a test using 0x01FC1F1D.
    Scan tests: 4, skipped: 0, failed: 0
    Do a test using 0x5533CCAA.
    Scan tests: 5, skipped: 0, failed: 0
    Do a test using 0xAACC3355.
    Scan tests: 6, skipped: 0, failed: 0
    All of the values were scanned correctly.
    
    The JTAG DR Integrity scan-test has succeeded.
    
    [End: Texas Instruments XDS2xx USB Debug Probe_0]
    

  • Create a new target configuration for your board & emulator, then try to connect the target and see gel is running.
    processors.wiki.ti.com/.../Target_Configuration_-_Custom_Configurations

    Also please make sure that you set boot mode to emualtion.