Hi,
A customer needs as many GPIO as possible on an AM437x design. I have seen some of the posts on AM335x and the necessity to have USB0_DRVVBUS connected.
Assuming VBUS0 is connected to 5V.
[] Could you confirm that USB0_DRVVBUS is necessary if the port is operated in Dedicated HOST mode (I think it is needed)
[] Could you confirm that USB0_DRVVBUS is necessary if the port is operated in Dedicated DRD mode (I think it is needed)
[] Could you confirm that USB0_DRVVBUS is necessary if the port is operated in Dedicated DEVICE mode (I don't think it is needed)
Thanks,
--Gunter