Hi,
we are working with the DM8168 running on a custom board. In an current project, we want to use the DM8168 only for configuring the surrounding interfaces. This is done right after the boot phase is finished. After that we would like to disable as much as possible from the DM8168 to minimize the heat production. I've tried to do that but I can't see any decreasing power consumption. I've checked the CPU usage using the "top" command. I could see a CPU usage of only 1%. So why is the DM8168 consuming the same amount of power regardless on the CPU load?
I'm looking forward for any response.
Thanks a lot.