Hi experts,
my board: EVMK2H Rev 40
SoC : TCI6638K2K
MCSDK: MCSDK_bios_3_01_00_03
I use the UART test code of the platform_test.pjt in PDK package.
The code seems to have problems, so the platform can not correctly receive data from an external computer.
After I study and run code ,I think that this example is not complete.
Is this an example of UART which can run for first TX and then RX ?
Does it miss the UART_reset function?
Could you provide relevant examples for me, please?
Thanks!
Brian