This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Artefacts on screen when mouse is moving. What is the problem?

I use the latest version of am335x SDK. I run my QT application or QT applications from Matrix GUI on Beaglebone Black I have artefacts on display when mouse is moving. When mouse not connected all is ok. I also noticed that the led indicator of CPU activity is shines much brighter during the cursor is moving.  I also do not sure that SGX in the CPU is used. The utility "System Information" from "Matrix GUI" says "SGX Core version:  Unknown or not present". It is strange because in SDK release notes says that SGX is used. What is the problem?