Do the K2H and K2L have different versions of the Network Coprocessor (NETCP) peripheral and underlying Packet Accelerator (PA), Security Accelerator (SA), gigabit Ethernet switch (GbE)?
Looking at the data sheets available on the product pages on the TI site, it seems to indicate that they do have different versions of the NETCP. The K2H page points to older (Keystone 1?) documents for NETCP, PA, SA, etc. The K2L page has links to documents for newer versions of NETCP, PA2, SA2, etc. These documents also only mention K2L and K2E processors and do not mention K2H.
Based on this, is it it accurate to say that the K2L has a newer NETCP subsystem than K2H, even though they are both Keystone 2 chips?