Other Parts Discussed in Thread: OMAP-L137
Hello
Usually connecting to the mentioned board with CodeComposerStudio was no problem, now that i tried to run one of the test-programs available on the download-page (LED-Test) the connecting to the board, while starting CSS (v3.3) does not work anymore.. the whole message is :
Error connecting to the target: Error 0x80000240/-1180 Fatal Error during: Initialization, OCS, The target is stuck in Wait-in-Reset mode. The applied reset must be released before progressing.
It seems that one of my co-workers "accidentially" pushed the SW4 Reset Switch.
Can this be the reason for the conection not to work?
Can you please tell me how to "un-reset" the board ?
So, which informations have been lost?
And how can i bring them back.
it would be nice do get detailed how-to-do-Instructions, because i am wether familiar with the bord, nor with Linux (like the one delivered on the SD card), thanks for your help
best regards Rico