This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138

Hello!

     I'm reading a paper on wiki (processors.wiki.ti.com/.../OMAP-L138_LCDK_Linux_Software_Developer's_Guide )  rencently and i got a question.In this paper,there are some words I do not understand.

Command prompts in this guide

Commands are preceded by prompts that indicate the environment where the command is to be typed. For example:

host $

Indicates command to be typed into the Linux host shell comand line of the host Linux workstation.

EVM #

Indicates commands to be typed into the U-Boot shell command line from the console window connected to the LCDK board’s serial port.

target $

Indicates commands to be entered into LCDK Linux shell command line, which is usually the serial terminal window connected to the LCDK board's serial port.

I will very appreciate it if you can tell me what is the U-Boot shell command line and what is the LCDK Linux shell.

Regards,

    Sai.