Hi,
Operating temperature of this part TMX320DM8168ACYG is only from 0°C ~ 95°C. Do you have the same part in the temperature range of -40 to 125degC , Since our end appilcation is in Aircraft. if dont have the same part in that temperature please suggest the alternate with our required military standard temperature in TI. Thanks.