Hi,
I'm facing a problem where I have to get a frame for analyses in a period of 200ms.
My board was made using like reference the EVM6437.
At my board I have a TVP5146 configured for two video inputs (CVBS NTSC) selecting by I2C, and I'm using a DSP6437-400Mhz.
The problem is that, sometimes the video captured are mixed between the two inputs.
I have already tried to change in a higher period of time like 500ms and it's worked well. But I really need to work with 200ms or less.
Someone could help me with an idea?