Hello,I'm building the Linux kernal for OMAPL38 LCDK refer to this paper ( http://processors.wiki.ti.com/index.php/OMAP-L138_LCDK_Linux_Software_Developer%27s_Guide#Steps_to_export_an_NFS_mount )
when entering the command ' ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi- make uImage ' in host command line,something goes wrong.
The host command line reply
' make : arm-arago-linux-gnueabi-gcc : command not found
CHK include/linux/version.h
CHK include/generated/utsrelease.h
make[1]: "include/generated/mach-types.h" is the latest
CC kernel/bounds.s
/bin/sh : 1 : arm-arago-linux-gnueabi-gcc : not found
make[1] : [kernel/bounds.s] error 127
make: [prepare0] error 2 '
I don't think it is because of the problem of GCC Tool Chain's path,for theformer command
' host $ ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi- make menuconfig' executed successfully.
Regards,
Sai.