We need to burn a bootable linux image into NAND flash on a custom target board with 66A2KH12.
Please verify that the method to construct a bootable image is as follows (MCSDK UG, p. 71 and following): U-Boot Build instructions, Boot Monitor Build instructions, Linux kernel and the device tree blob build instructions, TransportNetLib Software Library and Build instructions
Also, please verify that the program_evm script located in the mcsdk_bios_3_xx_xx_xx/tools/ directory is the best tool for this?
Thanks,
Bruce