Hi,
I use idkam437x with ccs 6.1.2, sysbios 6.45.1.29, sdk 2.1.1.2 and ndk 2.24.3.35.
I would like to establish a standard ethernet connection via tcp/ip transmission&stack by the use of PRUICSS module. There are two network examples in sdk: ethernet_mac and ethernetip_adapter. There is one nice example in pdk called NIMU_ICSS_BasicExample_idkAM437x_wSoCLib_armExampleproject, but it is almost a copy of ethernet_mac example. I have established two IP addresses at PHYs connected to PRU0 and PRU1 - it seems to be working so far.
Now there is another step related to the network connection: I would like to send and receive some data through the link - unfortunately none of the examples mentioned provides the transmission handling. Could you please give me some hints where should I look for the transmission API? Is it located in the vicss_emacDrv.h file where most of the ICSS_EMAC interface belongs?
Thanks
JJ