This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Linux DRM cannot save screen

On other Linux machines using the FBDEV drivers ( Raspberry Pi.. etc. ), I could mmap the /dev/fb0 device and directly create a BMP file that saved what was on the screen.

Now, I am trying to do the same thing with DRM on a TI Sitara AM57XX ( Beagleboard X-15 ). The code that used to work with FBDEV is shown below.

This mmap no longer seems to work the DRM. I'm using a very simple Qt5 Application with the Qt platform linuxfb plugin. It draws just fine into /dev/fb0 and shows on the screen properly, however I cannot read back from /dev/fb0 with a memory mapped pointer and have an image of the screen saved to file. It looks garbled like this:

Code:

#ifdef FRAMEBUFFER_CAPTURE

repaint();
QCoreApplication::processEvents();

// Setup framebuffer to desired format
struct fb_var_screeninfo var;
struct fb_fix_screeninfo finfo;
memset(&finfo, 0, sizeof(finfo));
memset(&var, 0, sizeof(var));
/* Get variable screen information. Variable screen information
* gives information like size of the image, bites per pixel,
* virtual size of the image etc. */
int fbFd = open("/dev/fb0", O_RDWR);
int fdRet = ioctl(fbFd, FBIOGET_VSCREENINFO, &var);
if (fdRet < 0) {
qDebug() << "Error opening /dev/fb0!";
close(fbFd);
return -1;
}

if (ioctl(fbFd, FBIOPUT_VSCREENINFO, &var)<0) {
qDebug() << "Error setting up framebuffer!";
close(fbFd);
return -1;
} else {
qDebug() << "Success setting up framebuffer!";
}

//Get fixed screen information
if (ioctl(fbFd, FBIOGET_FSCREENINFO, &finfo) < 0) {
qDebug() << "Error getting fixed screen information!";
close(fbFd);
return -1;
} else {
qDebug() << "Success getting fixed screen information!";
}

//int screensize = var.xres * var.yres * var.bits_per_pixel / 8;
//int screensize = var.yres_virtual * finfo.line_length;
//int screensize = finfo.smem_len;
int screensize = finfo.line_length * var.yres_virtual;
qDebug() << "Framebuffer size is: " << var.xres << var.yres << var.bits_per_pixel << screensize;
int linuxFbWidth = var.xres;
int linuxFbHeight = var.yres;

int location = (var.xoffset) * (var.bits_per_pixel/8) +
(var.yoffset) * finfo.line_length;

// Perform memory mapping of linux framebuffer
char* frameBufferMmapPixels = (char *)mmap(0, screensize, PROT_READ | PROT_WRITE, MAP_SHARED, fbFd, 0);
assert(frameBufferMmapPixels != MAP_FAILED);

QImage toSave((uchar*)frameBufferMmapPixels,linuxFbWidth,linuxFbHeight,QImage::Format_ARGB32);
toSave.save("/usr/bin/test.bmp");
sync();

#endif

Here is the output of the code when it runs:

Success setting up framebuffer!
Success getting fixed screen information!
Framebuffer size is: 800 480 32 1966080

Here is the output of fbset showing the pixel format:

mode "800x480"
geometry 800 480 800 480 32
timings 0 0 0 0 0 0 0
accel true
rgba 8/16,8/8,8/0,8/24
endmode

root@am57xx-evm:~#

[1]: i.stack.imgur.com/VJ96D.png