Hi,
I am using the AWS SDK with the CC3200 launchpad, I am able to compile and flash the code using the uniflash to the target( CC3200 launchpad ), but every time when I run the board not every time it is connecting to the aws, at least I need to try 4 to 5 times nby resetting the system then only it is able to connect to the aws server after that it works fine, but again in next restart it is taking 4-5 time to connect to Internet. I ran the aws sdk code in Linux environment with the same credentials and found every time that is working fine.
Note: here I am getting this message before it is getting failed, "startNTP: NTP host cannot be resolved!"
Please suggest what is going wrong here.
Thank you.
regards,
Zafar