Advisory 1.2.4 of the errata document for TMS320DM365 Silicon Revision 1.1 and 1.2 describes an ECC issue that seems to be related to the condition where more than 4 errors are found. The advisory describes the code changes that address this issue which have been incorporated into the latest release.
One of the e2e forum posts (see links below) describes an ECC issue which seems to be timing related (i..e. the ECC has not finished its calculations before other process are initiated.) Code modifications which supposedly address this issue are given at the end of the thread.
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/p/266652/935165
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/p/182730/708236.aspx#708236
Question 1. Are these two different issues that require two different code changes? Or are they both addressed by the code changes described in Advisory 1.2.4 of the errata?
Question 2. If they are different issues, has the timing-related ECC issue been addressed in the latest release?
Thanks,
Chris