Hi,
I have the K2H set up for NAND boot by placing 0x106E7 in DEVSTAT. I create a H/W watchpoint on read from 0x30000000 which is where NAND flash resides. I enable "Halt on Reset, then I reset the CPU. The PC goes to 0x00000000. Everything should be good. Then I run, but the H/W watchpoint never triggers, and the PC ends up in a loop at 0x000009D8. That is the same address as it end up in "No Boot" mode.
Please help!
Thanks,
Bruce