Other Parts Discussed in Thread: OMAPL138
When I boot OMAPL138 (not EVM), after showing "omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0"
the system stoped.
I've add "TI RTC" support in the kernel ( 2.6.32)
This is my uboot msg:
U-Boot 2009.08 (May 06 2010 - 21:32:23)
I2C: ready
DRAM: 64 MB
NAND: NAND device: Manufacturer ID: 0xec, Chip ID: 0xd3 (Samsung NAND 1GiB 3,3V
8-bit)
Bad block table found at page 524160, version 0x01
Bad block table found at page 524032, version 0x01
1024 MiB
*** Warning - bad CRC or NAND, using default environment
In: serial
Out: serial
Err: serial
ARM Clock : 84000000 Hz
DDR Clock : 72000000 Hz
Error - unable to probe SPI flash.
Net: Ethernet PHY: GENERIC @ 0x00
Hit any key to stop autoboot: 0
the arm clock is not 300MHz, does it cause the failure? My hareware is still with some problems, so I can't set the freq to 300MHz, I set the freq in arm-ubl side.
Another problem:
why it show bad block?