This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am437x without DDR3



Hi all

we are developing Ethercat slave device using AM437x and Beckhoff SSC stack code.currently I m ruining our source code on am437x IDK. the current code size is less than 240KByte. 

I read many E2E threads which are using am335x without DDR3 

since we are developing a very cost sensitive application,I wondered is it possible to design am437x custom board without a DDR3????

Based on am437x spec we suppose to have 512kBytes of memory.which suppose to be enough.

www.ti.com/.../AM4379

On-Chip Memory (Shared L3 RAM)

  • 256KB of General-Purpose On-Chip Memory 
    Controller (OCMC) RAM
  • Accessible to All Masters
  • Supports Retention for Fast Wakeup
  • Up to 512KB of Total Internal RAM 
    (256KB of ARM Memory Configured as L3 RAM 
    + 256KB of OCMC RAM)

So please let me know if any of your customer attempted mentioned configuration?

thanks in advance.