Other Parts Discussed in Thread: AM3359
Hello,
Our custom AM3359 board, using TPS65217B demonstrates the following strange behaviour: when the UART0 Tx pin is connected to a host's serial port, then power-off (software or via PMIC power button) works properly. If the Tx pin is not connected, the board power-cycles a few seconds after the power-off event. It seems that the connection of the Tx pin provides some adequate bleed off to allow voltage levels to drop during power-off. But we have not managed to identify the root cause of the issue. Any ideas would be appreciated.
We have the same behaviour in all kernels we have tried (ranging from 3.2.33 to 4.1.10).
Thank you.
Best regards,
Nikos