Other Parts Discussed in Thread: OMAP3530
I'm using an omap3530, and I need some sort of audio encoding support-- either MP3 or AAC. I've done MP3 on the ARM side, but it uses too much CPU.
From the TI Digital Media Software Inventory, it looks like AAC is my only option. I've downloaded c64xplus_aacldenc_1_00_00_000_production.bin and extracted it, but it seems difficult to get this integrated into my ti-codecs-omap3530_1.00.01.bb recipie (I'm using openembedded).
Are these the only instructions available? http://processors.wiki.ti.com/index.php/How_do_I_Integrate_new_codecs_into_DVSDK
If I manage to get it integrated, will all I have to do is replace my existing cs.x64P on the target with the new one? Will the ti gstreamer plugin work with the aac encode codec, or does it need changes as well?
Also, I found references to a "mega server" in the DVSDK 3.01.00.10 notes. It seems to have more codecs, including aac encoding, but I'm confused as to why it would be created instead of just integrating the new codecs into the existing "combo". DVSDK 3.01.00.10 is not available yet?