This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x: VTP_CTRL register wrong reset value



Hi there,

we observed that the filter bits on position 3:1 in VTP_CTRL register are "011" after a cold reset. According to the TRM, the reset value should be "000".

Is the reset value in the TRM correct?


Regards

  Wolfram Stumpf