Other Parts Discussed in Thread: CC2640
Hi,
I am working on a CC2640 custom 4x4 board, TIRTOS 2.13, BLE stack 2.1, CCS 6.1.2.
I added the UART driver in read callback mode to SimpleBLEPeripheral.c in order to process
every UART read through the RTOS queue.
In defining the UART writeMode parameter-- Can the UART write be blocking mode or does
this also have to be callback mode? If both the UART read and write have to be callback,
I need to think about the callback processing through the RTOS queue differently. I
need the UART read and write to be an asynchronous process that repeats for some time
during the application.
Thanks,
Priya