This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

about download of the files from the net



hi paul .....

sorry i didn't reach you these many days.

i have a problem with downloading the files from the internet using terminal.

generally from   Linux we can download files using the command "wget <path of file>"

same command i used for download files from the net there is two ways i followed 

1---------------->

root@10.0.0.7:/opt/dvsdk# wget http://ftp.gnu.org/gnu/wget/wget-1.6.tar.gz

--12:16:16--  http://ftp.gnu.org/gnu/wget/wget-1.6.tar.gz
           => `wget-1.6.tar.gz.1'
Resolving ftp.gnu.org... failed: Temporary failure in name resolution.

but i am getting failed error because of resolution . i tried with ip address of the wed site

2------------------>

root@10.0.0.7:/opt/dvsdk# wget 140.186.70.20/gnu/wget/wget-1.6.tar.gz

--12:16:31--  http://140.186.70.20/gnu/wget/wget-1.6.tar.gz
           => `wget-1.6.tar.gz.1'
Connecting to 140.186.70.20:80... connected.
HTTP request sent, awaiting response... 200 OK
Length: 670,777 (655K) [application/x-gzip]

100%[====================================>] 670,777      133.63K/s    ETA 00:00

12:16:38 (121.21 KB/s) - `wget-1.6.tar.gz.1' saved [670777/670777]

now it is working fine

--------------------------------------------------------------------------------------------------------------------------

please tell me how to work the first case . because remembering the ip address is so hard .

 

 

thanks  for your support on all my issues