Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hello,
Right now I am using the "Omap L138-EVM Kit provided by Ti". I am trying to clone the BSP provided by them and rebuild an Win CE using visual studio.
I have problem selecting both SD host controller and Nand Flash. I am not able to enable both at a time. So,my WINCE doesn't detect SD card even though there is an SD card slot in the EVM kit.
Can you tell me if there is a way to edit the BSP , so that it lets me enable both the SD and Nand flash together.
Am having the conflict with the pin mux of SD and NAND. The nand which we are using is 8bits . but the bsp which have 16bits . how to make changes. Could anybody help me to reduce the 16bits nand to 8bit nand . so that i can able to select both together.
Regards
Vinoth.