This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to add LCD support in L138

Other Parts Discussed in Thread: OMAPL138

I've a OMAPL138 board ( not EVM ) and I can boot the linux kernel now. But the LCD is not open. So I want to add LCD support in U-Boot & the kernel. First, I add the RASTER_init function in the u-boot. and the LCD seems light, but it always blinking. and the picture is also wrong. e.g. I want to show: RRRGGGBBBB RRRGGGBBBB RRRGGGBBBB It may show RRRGGGBBBB RRGGGBBBBR RRGGGBBBBR And when unpressing kernel is done, the LCD close again. How could I add the LCD in kernel? I don't know which folder should I modify. Thanks