Hi,
I have some questions regarding the frequency value when DVFS using. Please see the below.
1) What is the minimum frequency for each VD_xxx(VD_MPU, VD_DSPEVE, VD_IVA, VD_GPU, VD_CORE and VD_RTC) when DVFS feature using? Is it the frequency that is specified as OPP_NOM? If minimum frequency is not same as OPP_NOM frequency, please let me know the minimum frequency for each power domain(VD_xxx).
2) What is the minimum voltage for each VD_xxx when DVFS using? Is it the MIN voltage that is specified as MIN voltage of OPP_NOM in AM5728 data manual Table 5-7? If minimum voltage is different from MIN value, please let me know its value.
3) According to AM5728 TRM - 3.1.2.3 Dynamic Power Switching, it is written in the below.
When DPS is applied, a processor or system runs at the highest OPP
(maximum frequency and voltage) to complete its tasks quickly, followed by an automatic switch to a low-
power mode for minimum power consumption. DPS is useful when a real-time application is waiting for an
event.
If the processor will work OPP_NOM setting (not OPP_OD, OPP_HIGH), how probability is the power consumption reduced? Is this any enough merit to use DPS. Of course, I know current Linux SDK does not support DPS.
Please advise me.
I appreciate your quick reply.
Best regards,
Michi