HI,
Sorry for my English.
I used the ti-processor-sdk-linux-am335x-evm-01.00.00.03 + TI Bluetooth Linux Add-On package on AM335 EVM GP
We test the BT with HandFree profile and then it's works well.
I have few questions as below,
1. when the HFP enabled , the BT is slave and CPU(host) is master , the CPU send the PCM clock 1.6Mhz and Fsync 16K to the BT , I want to adjust it ,but idont know how to do ? like PCM 512K & Fsync 8K .
2. As Item 1 , if I want to change the role that is BT as master and CPU as slave how to change it ?
3. When HFP enabled , I found the voice is too low from the audio jack , so how to increase the volume from the PCM on the am335
Nathan Kuo