Hi everyone,
I am looking for a platform to capture data from a cameralink compatible camera and do some signal processing. In other messages in this forum, it was stated that this would be possible. In order to test it, I plan to purchase the TMDXEVM8148 from Mistral.
Has anyone got any experience in that context? I would be interested to find out what is possible:
1) Is the cameralink interface capable of decoding data given a "base", "medium" or "full" link?
2) What is the maximum frame rate?
3) What is the supported bit width range?
4) Is there a cameralink physical connector on the EVM? If not, how difficult is it to connect a cameralink cable?
5) Is it possible to pass the video data to C6748 via DMA transfer?
6) Is it possible to program the EVM bare metal (TI-RTOS)?
Thank you and best regards
Hauke