Other Parts Discussed in Thread: SYSBIOS, TMS320F28035
Hi
I am using CCS 6.12 with SysBios 6.45.1.29. The platform is a custom board using TMS320F28035 and debugger pod is XDS100V2.
I am trying to port an existing non bios application to sysbios. I used an existing project for F28035 that uses semaphores and added my code and files to it. The code compiles and loads but upon run, it stops at ESTOP0 in the Rom area.
Very rarely it executes and runs beyond boot, thus running the LCD and rest of code.
What should I look for, or how to debug. Flash and Memory utilization is about 50 and 70 percent. The problem is only in this project. Other example projects of sysbios run fine.
I want to know and debug the problem bec otherwise i will not learn and will fall into the same pit some other time.
Regards
Jawwad