Hi,
I tried to boot the DM365 EVM board with the kernel I built and stored in the linux host via TFTP. The TFTP server is running fine. I follow the GSG and set the U-Boot variables as the following:
EVM # setenv bootcmd 'dhcp;bootm'
EVM # setenv serverip 141.213.15.236
EVM # setenv bootfile uImage
EVM # setenv bootargs mem=76M console=ttyS0,115200n8 root=/dev/mtdblock3 rw rootfstype=yaffs2 ip=dhcp video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,4050K dm365_imp.oper_mode=0 davinci_capture.device_type=4
EVM # boot
When the booting starts, I got the following message:
BOOTP broadcast 1
DHCP client bound to address 141.213.15.251
TFTP from server 141.213.76.39; our IP address is 141.213.15.251
Filename '\OSChooser\i386\startrom.com'.
Load address: 0x80700000
Loading: ## Warning: gatewayip needed but not set
T T T T T T T T T T T T T T T T T T T T
Retry count exceeded; starting again