Hi there, I have recently bought a OMAP-L137 EVAL board from Spectrum Digital and managed to get basic examples running on the board using CCS v3.3. I would like to use TI_RTOS with NDK on OMAP-L137 EVAL board, but I would like to use the latest CCS or at least CCS v6 because most of the support and training material I found on the web is based on CCS v5 or CCS v6.
I have installed CCS v6 but I am not able to find the target and platform information to C6747 in the target config settings. Please let me know if it is possible to using OMAP-L137 with CCS v6. Thanks.
Regards,
Mitesh