Hello all,
Currently I am working on AM3352 processor and I want to use DDR3 RAM.
In datasheet of AM3352 in section 7.7.2.3 they are mentioning that if 16 bit DDR3 is used then termination is not mendetory. Either we can use termination or we can make design without termination.
So my question is if I am using 16 bit DDR3 then how can I make such design in PCB in which I can use DDR3 with termination and without termination also.
I.E. as per datasheet in fig 7-47 & 7-48, If I am not using VTT termination then Can I make all Zo floating (refer figure 7-47)?
PCB routing Stub created in datalines before Zo can make any issue in in DDR3 communication? am3352.pdf