Dear all,
I have some questions in timing diagram. Does anyone can give me the answer, thanks.
- In the timing diagram, is the "nBE1/nBE0" means nBE1 divide nBE0 or something?
- Why there are two lines in the red square, and out of red square, there is only one line...?
- If i want to get the address data, i should use the nADV high/low signal to check, is that right?