Hi,everyone ,
I use C6678 EVM and want to configure MPAX register ,there is some questions as following :
In MPAXregister demo,the code as following :
lvMarPtr = (volatile uint32_t*)0x08000024;
H_Value = 0x90000017 ;
if (coreNum == 0) L_Value = 0x8100003f ;
if (coreNum == 1) L_Value = 0x8110003f ;
if (coreNum == 2) L_Value = 0x8120003f ;
if (coreNum == 3) L_Value = 0x8130003f ;
if (coreNum == 4) L_Value = 0x8140003f ;
if (coreNum == 5) L_Value = 0x8150003f ;
if (coreNum == 6) L_Value = 0x8160003f ;
if (coreNum == 7) L_Value = 0x8170003f ;
*lvMarPtr++ = L_Value;
*lvMarPtr++ = H_Value;
So we can see for MPAX register ,the value is different between coreNUM,After configure MPAX register above ,the 8 cores can use the same logical address and map to different physical address.and I have following questions :
1.It is possible to write the above code in IBL code ?I know ,only core 0 execute IBL code ,but above code configured MPAX register not only core 0 but also core 1~core 7.so I don't know how to confihure core1~core 7 MPAX register in IBL code as above code .
2.For PCIe boot,the linux PC will send project image to C6678,and the image included in .h file,is there some ways to complete 8 cores MPAX register configuration as above code before linux PC send the project image to C6678?
Thank you,
Simon