Other Parts Discussed in Thread: ADS62P45, OMAP-L138
Hi ,
i have a quesion about the Hawkboard.I want to connect the ADC (ADS62p45 EVM) to the UPP of the Hawkboard (OMAP-l138).
It might be that i have to design an adapter to connect between the parallel CMOS output of the ADS62p45 EVM and the UPP of the Hawkboard.
The problem which im facing right now is that the upp pins do not have so many mass pins as the cmos output of ADS62p45 EVM,which means i can't connect the mass of both Boards as 1 to 1.
Do you have idea how to connect the pins togeather.
If someone here can give me even pointers to that ,would be thankful
Kind regards
Moadh