This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718 IBIS model

Other Parts Discussed in Thread: AM5718

Hi,

I confirm AM571.ibs which is available from the following site.

www.ti.com/.../toolssoftware

Because there is the following ignorance point, please tell me.

What do 10 "PERCENT%" and 5" PERCENT%" mean in the following model choice of IBIS of AM5718 by SI simulation of MIPI?

[Model Selector] Selector_10
Model_752 I/O,1.8V,40D CLASS MODE FAST MODE,IND,10 PERCENT%,BC40D_V_10P_!SC1_1P8
Model_753 I/O,1.8V,40C CLASS MODE SLOW MODE,IND,10 PERCENT%,BC40D_V_10P_SC1_1P8
Model_754 I/O,1.8V,40D CLASS MODE FAST MODE,IND,5 PERCENT%,BC40D_V_5P_!SC1_1P8
Model_755 I/O,1.8V,40C CLASS MODE SLOW MODE,IND,5 PERCENT%,BC40D_V_5P_SC1_1P8

Best Regards,

Shigehiro Tsuda