Other Parts Discussed in Thread: TVP7002
Hi,
I was trying to boot the DM365 EVM using the kernel I built and file system in the host computer via TFTP and NFS as instructed in the GSG. It works fine.
Now when I just want to boot the board using the preloaded kernel and file system on the NAND flash, the boot failed and show bad blocks and kernel panic. Here is the booting message:
Jumping to entry point at 0x81080000.
LSP 2.10 BETA RELEASE
VERSION: 2.10.008.02
U-Boot 1.3.4 (Mar 2 2009 - 11:50:39)
I2C: ready
DRAM: 128 MB
NAND: NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
Bad block table found at page 524224, version 0x01
Bad block table found at page 524160, version 0x01
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
Bad block table found at page 524224, version 0x01
Bad block table found at page 524160, version 0x01
2048 MiB
In: serial
Out: serial
Err: serial
Ethernet PHY: GENERIC @ 0x00
Hit any key to stop autoboot: 0
Loading from NAND 1GiB 3,3V 8-bit, offset 0x400000
Image Name: Linux-2.6.18_pro500-davinci_evm-
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2026248 Bytes = 1.9 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.18_pro500-davinci_evm-
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2026248 Bytes = 1.9 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux.................................................................................................................
Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (a0850430@gtlnxlsf02.gt.design.ti.com) (gcc version 4.2.0 20070126 (prerelease) 9
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM365 EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0365 variant 0x8
PLL0: fixedrate: 24000000, commonrate: 121500000, vpssrate: 243000000
PLL0: vencrate: 27000000, ddrrate: 243000000, mmcsdrate: 121500000
PLL1: armrate: 297000000, voicerate: 99000000, vencrate: 74250000
MUX: initialized SPI0_SCLK
MUX: initialized SPI0_SDO)
MUX: initialized SPI0_SDI
MUX: initialized SPI0_SDENA0
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists. Total pages: 29696
Kernel command line: mem=116M console=ttyS0,115200n8 root=/dev/mtdblock3 rw rootfstype=yaffs2 ip=off davinci_capture.device_type=4 0
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 03
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 116MB = 116MB total
Memory: 113152KB available (3497K code, 712K data, 168K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 104 gpio irqs
DM365 IPIPE initialized in Continuous mode
Generic PHY: Registered new driver
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
LogicPD encoder initialized
Avnetlcd encoder initialized
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Mar 2 2009 12:21:46 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
davincifb davincifb.0: check_fb_var: calling convert_fb_var_to_osd, var->bits_per_pixel: 16
davincifb davincifb.0: convert_fb_var_to_osd: bits per pixel: 16
davincifb davincifb.0: davincifb_set_par: calling convert_fb_info_to_osd bpp: 16
davincifb davincifb.0: convert_fb_info_to_osd: var->bits_per_pixel: 16
davincifb davincifb.0: convert_fb_var_to_osd: bits per pixel: 16
davincifb davincifb.0: dm_osd0_fb: 720x480x16@0,0 with framebuffer size 675KB
davincifb davincifb.0: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 1020KB
davincifb davincifb.0: check_fb_var: calling convert_fb_var_to_osd, var->bits_per_pixel: 4
davincifb davincifb.0: convert_fb_var_to_osd: bits per pixel: 4
davincifb davincifb.0: davincifb_set_par: calling convert_fb_info_to_osd bpp: 4
davincifb davincifb.0: convert_fb_info_to_osd: var->bits_per_pixel: 4
davincifb davincifb.0: convert_fb_var_to_osd: bits per pixel: 4
davincifb davincifb.0: dm_osd1_fb: 720x480x4@0,0 with framebuffer size 675KB
davincifb davincifb.0: dm_vid1_fb: 0x0x16@0,0 with framebuffer size 1020KB
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
davinci_ldc initialized
imp serializer initialized
davinci_previewer initialized
davinci_resizer initialized
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfac20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfad06000 (irq = 41) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
netconsole: not configured, aborting
Davinci EMAC MII Bus: probed
MAC address is 00:0e:99:02:ce:e8
TI DaVinci EMAC Linux version updated 4.0
Linux video capture interface: v2.00
starting ccdc_reset...<7>
End of ccdc_reset...<5>vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = MT9T001
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = MT9P031
TVP514X : nummber of channels = 1
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = TVP514X
Trying to register davinci display video device.
layer=c72e9400,layer->video_dev=c72e9560
Trying to register davinci display video device.
layer=c72e9200,layer->video_dev=c72e9360
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = TVP7002
i2c /dev entries driver
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
2 NAND chips detected
Creating 5 MTD partitions on "nand_davinci.0":
0x00000000-0x00360000 : "bootloader"
0x00360000-0x003a0000 : "params"
0x003a0000-0x007a0000 : "kernel"
0x007a0000-0x207a0000 : "filesystem1"
0x207a0000-0x307a0000 : "filesystem2"
nand_davinci nand_davinci.0: hardware revision: 2.3
dm_spi.0: davinci SPI Controller driver at 0xc7866000 (irq = 42) use_dma=0
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
musb_hdrc: version 6.0, cppi-dma, host, debug=0
MUX: initialized GPIO33
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Host mode controller at c7868000 using DMA, IRQ 12
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
davinci-mmc davinci-mmc.1: Supporting 4-bit mode
davinci-mmc davinci-mmc.1: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
AIC3X Audio Codec 0.1
asoc: aic3x <-> davinci-i2s mapping ok
ALSA device list:
#0: DaVinci DM365 EVM (aic3x)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
yaffs: dev is 32505859 name is "mtdblock3"
yaffs: Attempting MTD mount on 31.3, "mtdblock3"
block 308 is bad
block 1335 is bad
block 1768 is bad
block 1967 is bad
block 2001 is bad
block 2044 is bad
block 2097 is bad
block 2154 is bad
block 2164 is bad
block 2174 is bad
block 2177 is bad
block 2202 is bad
block 2203 is bad
block 2219 is bad
block 2220 is bad
block 2221 is bad
block 2222 is bad
block 2223 is bad
block 2224 is bad
block 2225 is bad
block 2226 is bad
block 2227 is bad
block 2228 is bad
block 2229 is bad
block 2230 is bad
block 2231 is bad
block 2232 is bad
block 2233 is bad
block 2234 is bad
block 2235 is bad
block 2236 is bad
block 2237 is bad
block 2238 is bad
block 2239 is bad
block 2240 is bad
block 2241 is bad
block 2242 is bad
block 2243 is bad
block 2244 is bad
block 2245 is bad
block 2246 is bad
block 2247 is bad
block 2248 is bad
block 2249 is bad
block 2250 is bad
block 2251 is bad
block 2252 is bad
block 2253 is bad
block 2254 is bad
block 2255 is bad
block 2256 is bad
block 2257 is bad
block 2258 is bad
block 2259 is bad
block 2260 is bad
block 2261 is bad
block 2262 is bad
block 2263 is bad
block 2264 is bad
block 2265 is bad
block 2266 is bad
block 2267 is bad
block 2268 is bad
block 2269 is bad
block 2270 is bad
block 2271 is bad
block 2272 is bad
block 2273 is bad
block 2274 is bad
block 2275 is bad
block 2276 is bad
block 2277 is bad
block 2278 is bad
block 2279 is bad
block 2280 is bad
block 2281 is bad
block 2282 is bad
block 2283 is bad
block 2284 is bad
block 2285 is bad
block 2286 is bad
block 2287 is bad
block 2288 is bad
VFS: Mounted root (yaffs2 filesystem).
Freeing init memory: 168K
Warning: unable to open an initial console.
Kernel panic - not syncing: No init found. Try passing init= option to kernel.
What went wrong? Does that mean I actually overwrite the NAND flash when I boot via TFTP and NFS using the kernel and file system on the host? I thought this process does not overwrite anything on the NAND flash. Can someone please clarify this? Thanks.
Regards,
CW