This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359 ICEv2 switching between Profinet and EtherCAT

Other Parts Discussed in Thread: SYSBIOS

Hello,

would it be possible to combine Profinet slave and Ethercat slave functionality together in one project ? The goal is to make the board work with both worlds. For example, i connect the board to a Profinet PLC, toggle a GPIO via some kind of hardware switch to set the board into profinet mode and then turn the power on.  Then i take the same board, turn the power off, connect it to a ethercat PLC, toggle the GPIO via my hardware switch into ethercat mode and turn the power on.

Is this scenario possible? Maybe by combining the two example projects from sysbios ind sdk 2.1.1.2 ?

Or will there be conflicts in hardware or software ?

Thanks in advance

Michael