This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM571x GPMC performance with NAND Flash

Other Parts Discussed in Thread: AM5716

1. What is the maximum Read and Write speed achievable in AM5716 GPMC interface with ONFi NAND Flash

2. How many chip selects are supported by AM5716 GPMC for the external NAND Flash memory?

3. Boot Memory has to be connected to CS0 alone?

4. Our requirement is to use high ONFI_NAND Flash memory (2Tb to 4Tb) with higher through put (min. 83MB/Sec). What is the standard AM5716 supports for the NAND Flash interface like NV-DDR, NV-DDR2 or NV-DDR3?