This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6487 Boot from EMAC



Hello,

we have a DSP TCI6487+ connected to an Octeon processor using the  ETH interface.

On this architecure we boot the dsp using .eth file, and everything works.

Now we have to change the processor, so we need to recompile the program that  send the file .eth to DSP for the new processor.

Is it possibile to have the source file of this program? 

Regards,

Claudio

  • I've moved your post to the device forum.

    Todd
  • I think, .ETH source files are part of MCSDK releases for c64xx. I request you to see. I will check and get back. Thank you.
  • Please check the attached file.

    simple.zip

  • The .eth file are created starting for the .out file. I created it standalone.

    And every time the system starts follow this script:

    -----------------------------------------------

    echo Creating arpentries DSP1
    arp -s 192.168.16.31 00-24-BA-4E-5A-00

    echo arp creation for BS DSP1 done ...

    Packet.exe faraday_secboot.eth 192.168.16.31
    pause

    Packet.exe bsphy_dsp1.eth 192.168.16.31
    pause

    echo Emac Booting for BS DSP1 done ...!!!

    pause
    echo Creating arpentries DSP0
    arp -s 192.168.16.32 00-24-BA-4E-5F-C2

    echo arp creation for BS DSP0 done ...

    Packet.exe faraday_secboot.eth 192.168.16.32
    pause

    Packet.exe bsphy_dsp0.eth 192.168.16.32
    pause

    echo Emac Booting for BS DSP0 done ...!!!

    ----------------------------------------------------------

    I need is it possible the source file Packet.exe.

    If i understood how it works, should be send via UDP socket, the .eth file.
    Do you have this program or we have to do it by ourself?


    regards,
    Claudio
  • I checked simple.zip, but i do not understand what it does. I need the code on PC side to inizialize the DSP using ethernet interface.


    This is the script running on pc side:

    -----------------------------------------------

    echo Creating arpentries DSP1
    arp -s 192.168.16.31 00-24-BA-4E-5A-00

    echo arp creation for BS DSP1 done ...

    Packet.exe faraday_secboot.eth 192.168.16.31
    pause

    Packet.exe bsphy_dsp1.eth 192.168.16.31
    pause

    echo Emac Booting for BS DSP1 done ...!!!

    pause
    echo Creating arpentries DSP0
    arp -s 192.168.16.32 00-24-BA-4E-5F-C2

    echo arp creation for BS DSP0 done ...

    Packet.exe faraday_secboot.eth 192.168.16.32
    pause

    Packet.exe bsphy_dsp0.eth 192.168.16.32
    pause

    echo Emac Booting for BS DSP0 done ...!!!
  • Steps to send the simple.eth from the Host to the target DSP

    1. Boot the target DSP in ROM Ethernet boot mode.

    2. Once the DSP boots up, it transmits BOOTP packet at regular interval which will have the MAC ID of the DSP.

    3. Add an ARP entry for the DSP MAC address associating with an IP local to the host. For example if the host PC's

      IP is 192.168.1.1, then add an ARP entry with the DSP's MAC address associated with IP address 192.168.1.2.

    4. Use the pcsendpkt.exe to send the image to the DSP using the associated IP address. For example

      pcsendpkt.exe simple.eth 192.168.1.2  

    5. Use CCS to connect the EVM, and check that A1 register is set to 0x11223344, that confirms the simple program

      is received and booted by the ROM boot loader.

    Notes:

    1. In order to compile the pcsendpkt.c file please compile with -lwsock32 option for using windows socket.

    /******************************************************************************
     * Copyright (c) 2011 Texas Instruments Incorporated - http://www.ti.com
     *
     *  Redistribution and use in source and binary forms, with or without
     *  modification, are permitted provided that the following conditions
     *  are met:
     *
     *    Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     *    Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the
     *    distribution.
     *
     *    Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
     *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
     *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
     *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
     *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
     *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
     *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
     *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
     *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
     *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
     *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *****************************************************************************/
    
    #include <stdio.h>
    #include <stdlib.h>
    #include <time.h>
    #ifdef __WIN32__
    	#include <windows.h>
    	#include <winsock.h>
    #else
    	#include <sys/types.h>
    	#include <sys/socket.h>
    	#include <netinet/in.h>
    	#include <netdb.h>
    #endif
    
    
    #define UDP_LOW   42
    #define UDP_HIGH  1504  // Note: Windows FRAGMENTS higher UDP sizes
    
    #define SRCPORT   1234
    #define DSTPORT   9
    
    #define DELAY 60000
    
    /* convert ascii to decimal number */
    int toNum(unsigned char c)
    {
      if ((c >= '0') && (c <= '9'))
         return(c - '0');
    
      else  if ((c >= 'A') && (c <= 'F'))
    	  return(c -'A' + 10);
    
      else  if ((c >= 'a') && (c <= 'f'))
    	  return(c - 'a' + 10);
    
      return(-1);
    }
    
    
    int main( int argc, char *argv[] )
    {
    
    #ifdef __WIN32__
        WORD                wVersionRequested;
        WSADATA             wsaData;
        SOCKET              s;
    #else
    	int					s;
    #endif
    
        struct sockaddr_in  sin;
        unsigned char       *pBuf = 0;
        int                 tmp1,tmp2,tmp3,tmp4;
        time_t              ts,tn;
    	FILE *strin;
    	char iline[132];
    	int i,j,length;
    	int packetno;
    
        if( (argc != 3) ||
            sscanf(argv[2],"%03d.%03d.%03d.%03d",&tmp1,&tmp2,&tmp3,&tmp4)!=4 ||
            (tmp1 < 0 || tmp1 > 255 || tmp2 < 0 || tmp2 > 255 ||
             tmp3 < 0 || tmp3 > 255 || tmp4 < 0 || tmp4 > 255) )
        {
            printf("\nUsage: %s packetfile ipaddress\n",argv[0]);
            exit(-1);
        }
    
        tmp1 |= tmp2 << 8;
        tmp1 |= tmp3 << 16;
        tmp1 |= tmp4 << 24;
    
        strin = fopen (argv[1], "r");
        if (strin == NULL)  {
            printf ("could not open input file %s\n", argv[1]);
            exit(-1);
    	}
    
        /* Skip the first two lines */
        fgets (iline, 131, strin);
    	fgets (iline, 131, strin);
    
    #ifdef __WIN32__
        wVersionRequested = MAKEWORD(1, 1);
        tmp2 = WSAStartup(wVersionRequested, &wsaData);
        if (tmp2 != 0)
        {
            printf("\r\nUnable to initialize WinSock for host info");
            exit(0);
        }
    #endif
    
        s = socket( AF_INET, SOCK_DGRAM, 0 );
        if( s < 0 )
        {
    #ifdef __WIN32__
            printf("failed connect (%d)\n",WSAGetLastError());
    #else
    		perror("failed connect");
    #endif
            goto end;
        }
    
        sin.sin_family      = AF_INET;
        sin.sin_addr.s_addr = 0;
        sin.sin_port        = htons(SRCPORT);
    
        if ( bind( s, (struct sockaddr *)&sin, sizeof(sin) ) < 0 )
        {
    #ifdef __WIN32__
            printf("failed bind (%d)\n",WSAGetLastError());
    #else
    		perror("failed bind");
    #endif
            goto end;
        }
    
        /* Allocate a working buffer */
        if( !(pBuf = malloc( 2000 )) )
        {
            printf("failed packetno buffer allocation\n");
            goto end;
        }
    
        sin.sin_addr.s_addr = tmp1;
        sin.sin_port        = htons(DSTPORT);
    
        ts = time(0);
    
        packetno = 0;
    
        printf("\nSending packets to %d.%d.%d.%d\n",
                    tmp1&255, (tmp1>>8)&255, (tmp1>>16)&255, (tmp1>>24)&255 );
    
        while(1)
        {
    		/* get length in bytes */
    		if(fgets(iline, 131, strin)==NULL) break;
    	    length = toNum(iline[2])<<12 | toNum(iline[3])<<8 | toNum(iline[4])<<4 | toNum(iline[5]);
    		if(length == 0) break;
    		else if(length < UDP_LOW || length > UDP_HIGH) {
    			printf("Invalid length = %d\n",length);
    			goto end;
    		}
    
    		/* skip the next 21 lines, 14 mac + 20 IP + 8 UDP = 42 bytes = 21 lines */
    		for(i=0; i<21; i++) {
    			if(fgets(iline,131,strin)==NULL) break;
    		}
    
    		length -= 42;
    		if(length < 0) {
    			printf("Invalid length = %d\n",length);
    			goto end;
    		}
    
    		/* copy the payload: magicno + seq no + boot table */
    		for(i=0,j=0; i< length/2; i++) {
    			if(fgets(iline, 131, strin)==NULL) break;
    
    			*(pBuf+j) = toNum(iline[2])<<4 | toNum(iline[3]);
    			j++;
    			*(pBuf+j) = toNum(iline[4])<<4 | toNum(iline[5]);
    			j++;
    		}
    
    		/* send out the packet */
            if( sendto( s, pBuf, length, 0, (struct sockaddr *)&sin, sizeof(sin) ) < 0 )
            {
    #ifdef __WIN32__
            printf("send failed (%d)\n",WSAGetLastError());
    #else
    		perror("send failed");
    #endif
                break;
            }
    
    		/* packet number */
            packetno++;
    		printf("Packet %d sent\n",packetno);
    
    		/* add delay between packets */
    		for(i=0; i<DELAY; i++) {
    			tmp4 = tmp3;
    			tmp3 = tmp4;
    		}
    
    		/* skip the next two lines */
    	    if(fgets (iline, 131, strin)==NULL) break;
    		if(fgets (iline, 131, strin)==NULL) break;
        }
    
        tn = time(0) - ts;
        printf("Exiting . Time = %d seconds, Total Packets = %d\n",(int)tn,packetno);
    
    	/* clean up */
    end:
    	fclose(strin);
    
        if( pBuf )
            free( pBuf );
        if( s >= 0 )
    #ifdef __WIN32__
            closesocket( s );
    #else
    		shutdown(s,SHUT_RDWR);
    #endif
    
    #ifdef __WIN32__
        WSACleanup();
    #endif
    }
    
    

    Thank you.