Dear All,
Does AM437x support DDR2 ?
I have checked the following doc and datasheet, says that it does support LPDDR2 and DDR3 but I want to know whether it could support DDR2 or not ?

I have got the following content from AM437x Data sheet, page no 199
When not using a part of LPDDR2 interface (using x16 or not using the LPDDR2 interface):
• Connect the VDDS_DDR supply to 1.8 V
• Connect the DDR_VREF supply to 0.9 V
• Tie off DDR_DQS[x] (x=0,1,2,3) that are unused to VSS via 1 kΩ
• Tie off DDR_DQSn[x] (x=0,1,2,3) that are