This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM437x OTG Functionality

I have a AM437x on a custom dev board with a usb port and I want to be able to plug in and use USB OTG devices.  I understand the necessary hardware changes needed to accomplish this, but I am confused about whether or not the AM437x can actually support USB OTG devices while acting as a host.  According to the TRM, the AM437x does not support USB OTG functionality.  Oddly though, it supports Dual Role Device - Host or Device modes; what is the difference?  I have also seen others post about enabling OTG functionality on the AM437x like this post for instance.  Can somebody explain if the AM437x can or cannot support USB OTG?