This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x: I2C in polling mode does not send data

Genius 5820 points


Hi,

I try to access a I2C device in polling mode but until now without any success. Only one byte 0x3C is sent and this byte does not have to do anything with the data I try to transmit. So that's what I'm doing at the moment:

Initialisation:

  • set up correct PIN-muxing
  • set up I2C1 module clock
  • disable I2C by clearing EN-bit in register I2C_CON
  • reset I2C by setting bit SRST in register I2C_SYSC
  • disable auto-idle mode by celaring bit AUTOIDLE in register I2C_SYSC
  • set the I2C clock to 400 kHz
  • set own address 1 in register I2C_OA
  • enable I2C by setting EN-bit in register I2C_CON
  • wait until bit RDONE in register I2C_SYSS is set to see if reset of I2C was completed
  • set mode "Master" and "Transmit" my setting bits MST and TRX in register I2C_CON
  • set slave-address 0x1E by writing it into register I2C_SA

Then transmission is done this way:

  • set the number of bytes (3) to be transferred by writing them into register I2C_CNT
  • read back register I2C_CNT to see what amount of bytes really can be transferred
  • wait for bus being free by waiting for bit BB in register I2C_IRQSTATUS_RAW going to 0
  • initiate for transfer by writing bits STT, STP, TRX and MST into register I2C_CON
  • now in a loop until all three bytes have been sent:
    • wait until bit XRDY in register I2C_IRQSTATUS_RAW is set
    • write next data byte to be transmitted into register I2C_DATA
    • write a 1 into bit XRDY in register I2C_IRQSTATUS_RAW to clear the XRDY state

This whole procedure does not result in a valid data transmission. So what could be wring here?

PS: I'm asking this question independent from any software platform, I'm doing this with my own implementation, so this is not specific to any TI software.