Hello,
It seems that different USB camera the AM335x based system (based on Kernel 4.1.18) freezes at some point without giving any logs.
Here are some comments on the crash:
- No crashes when disabling the uvcvideo kernel module.
- No crashes not having webcam connected.
- There is not difference in crashing between DMA and PIO mode for USB.
- There is no logging before the system freezes (not in dmesg, not via an GPIO debug header).
Could you please clarify :
-what uvcvideo USB uses case have been validated with kernel 4.1.18?
-what web cam was used for testing?
- What test code was used to test the USB webcam use case?
Some further details will be posted soon.
Thanks in advance,
Anthony