Other Parts Discussed in Thread: OMAP3530
Hi,
I have one question about cache availability on Beagle board.
We are using Beagle Board B4, running Angstrom linux uImage version 2.6.28.
While we compare the performance of our codecs on Beagle Board with the performance of our codecs on other devices with Cortex-A8 CPU (e.g. iPhone 3GS), there is significant difference in performance (iPhone has much better performance). I suspect that the L1/L2 I/D cache are not enabled on Beagle/Angstrom or full size of cache are not enabled. But i have no way to find out.
I am aware that OMAP3530 has following cache for Cortex-A8:
L1: 32 KB (I+D)
L2: 256 KB (D)
Is there a way that we can see information about cache sizes on beagle board/Angstrom.
Thanks & regards,
Garima